BLE_HOGPS_SetBootKeyboardOutputReport
C
uint16_t BLE_HOGPS_SetBootKeyboardOutputReport(uint8_t ledValue);
Description
Sets the output report for a HID boot keyboard.
Note
This function updates the LED status indicators on a HID boot keyboard, such as Num Lock, Caps Lock, and Scroll Lock LEDs. The state of each LED is represented by individual bits within the provided 'ledValue' parameter.
Parameters
Parameter | Description |
---|---|
[in] ledValue | A bitmask where each bit corresponds to an LED on the keyboard:- Bit 0: Num Lock LED- Bit 1: Caps Lock LED- Bit 2: Scroll Lock LED- Bit 3: Compose LED- Bit 4: Kana LEDBits 5 to 7 are reserved and should be set to 0. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | The output report was successfully set. |
MBA_RES_INVALID_PARA | The input parameters are invalid. |