BT_SYS_Init
C
bool BT_SYS_Init(void *p_reqQueueHandle, void *p_osalApiList, BT_SYS_Option_T *p_option, BT_SYS_Cfg_T *p_cfg);
Description
Initialize the Bluetooth system.
Parameters
Parameter | Description |
---|---|
[in] p_reqQueueHandle | Handle to the OS queue for Bluetooth internal task management. |
[in] p_osalApiList | Pointer to the list of OS abstraction layer (OSAL) APIs. |
[in] p_option | Pointer to the structure containing initialization options. See BT_SYS_Option_T. |
[in] p_cfg | Pointer to the structure containing system configuration parameters. See BT_SYS_Cfg_T. |
Return values
Return value | Description |
---|---|
true | Successfully initialize Bluetooth system. |
false | Fail to initialize Bluetooth system. |