3.11.2 Getting Started Application using Harmony v3 Drivers on SAM E70 Xplained Ultra Evaluation Kit
Description
The application reads the current room temperature from the temperature sensor on the I/O1 Xplained Pro Extension Kit. The temperature reading is displayed on a serial console periodically every second. Further, the application writes the temperature readings to EEPROM. When a character is entered on the console, the last five written temperature values are read from the EEPROM and displayed on the console. The LED (LED3) is toggled every time the temperature is displayed on the serial console.
Modules/Technology Used
- Peripheral Modules:
- PORTS
- USART
- Timer
- XDMAC
- Drivers:
- TWIHS (I2C)
- USART
- System Services:
- Timer
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e70_xult.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Verify that the temperature sensor (I/O1 Xplained Pro Extension Kit) is connected to Extension Header 1 (EXT1) on the SAM E70 Xplained Ultra Evaluation Kit.
- The SAM E70 Xplained Ultra Evaluation
Kit allows the Embedded Debugger (EDBG) to be used for debugging. Connect the Type-A
male to micro-B USB cable to the micro-B DEBUG USB port to power and debug the SAM E70
Xplained Ultra Evaluation Kit.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME70Q21B.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (getting_started_drv\firmware\drivers_sam_e70_xult.X) in MPLAB X IDE
- Ensure SAM E70 Xplained Ultra is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program Device button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button).
- Change the baud rate to 115200.
- The user should see the temperature
values (in °F) being displayed on the terminal every 500 milliseconds, as shown
below.

- Notice the LED3 blinking at 1 second rate.
- Press any character on the terminal
to display the last five values written to the EEPROM.
- The user may vary the temperature by
placing the finger on the temperature sensor (for a few seconds).
Comments
- Reference Training Module: Getting Started with Harmony v3 Drivers and System Services on SAM E70/S70/V70/V71 MCUs
- This application demo builds and
works out of box by following the instructions above in "Running the Demo"
section. If the user needs to enhance/customize this application demo, the user needs
to use the MPLAB Harmony v3 Software framework. Refer links below to setup and build
the applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project