If the target is powered through the debugger with an externally powered
hub as shown below, the power available to the target is limited to 50 mA.Figure 3-5. Target Powered Through Self-Powered Hub
Not all devices have the AVDD and AVSS lines, but if they are
present on the target device, all must be connected to the appropriate levels in order
for the debugger to operate. They cannot be left floating.
Also, devices with a VCAP line (PIC18FXXJ for example) should be connected to
the appropriate capacitor or level.
Note: The interconnection is very simple. Any problems experienced are often caused by other
connections or components on these critical lines that interfere with the operation of
the MPLAB PICkit 4 In-Circuit Debugger, as discussed in
the following section.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.