6.4.2 Reportlog File Format
The RLM servers create a reportlog in three formats, selectable by the License Administrator. The three formats are “std”, “small”, and “detailed”.
Note that prior to RLM v9.3 there was no “detailed” format on Windows; specifying “detailed” would produce a standard report output. Starting in RLM v9.3, the detailed report will be produced, but all fractional seconds fields will be 0.
The formats differ only in the contents of the checkout and check-in records, as described below. Common to all formats are the classes of data logged, and the data for all except check-in and checkout records.
The reportlog format has a version number in the start record. All data described applies to all versions of the reportlog, except where indicated.
The data is:
- authentication data
- check-in
- checkout
- dequeue
- dynamic reservation created/removed (added in RLM v12.2)
- isv-specific data
- license denial
- license in use (added in RLM/reportlog v10.0)
- log file start
- log file end (can correspond to a switch to a new logfile)
- meter transaction data (added in RLM v9.3)
- periodic timestamps
- queue
- roam extend
- server shutdown
- server time jumped
- server reread of license/option file
- support for a product (feature) - one for each license pool at log file start time
- temporary license creation/removal (added in v14.1 – RLM Cloud servers only)
A reportlog consists of the following data:
- log file start records
- one PRODUCT support line for each supported product
- one license in use record for each currently-checked-out license
- all license activity data, including checkouts, check-ins, AUTH records, etc.
- one license in use record for each currently-checked-out license
- optional SWITCH line
- END line
- final AUTH line
The format of the data logged is described in the following sections.