6 Example Applications
The host example applications provide few examples to demonstrate the RNWF02 features and capabilities. These set of applications are based on
AVR128 Host MCU. These examples use the following development tools:Figure 6-1. Host Companion Mode
- AVR128DB48 Curiosity Nano Evaluation Kit (EV35L43A)
- Curiosity Nano Base for Click boards™ (AC164162)
- RNWF02 Add On Board Early Access Kit (EA32M85A)
- SQI SUPERFLASH® KIT 1 (AC243009)
These example applications can be downloaded or cloned by any one of these methods:
- From the RNWF
GitHub page, download the ZIP file. As illustrated in the following
figures:Note: Ensure to select the latest version in Tags
Figure 6-2. Downloading the ZIP file Figure 6-3. Downloading the ZIP file - Using Git CMD, for more details on using GitBash, refer to the 3.1.8.1 Cloning the Application section.