5.8 Tunneling in Secure Networks

Consider a network wherein a node insecurely joins through a router parent, and the joining node does not know the network key prior to the join procedure. In this case, using the APS command to securely communicate the network key from the trust center to the newly joined router is called the APS tunnel command.

The end-device 0x0beeLL joins router 0x3c08 from packet #89. The parent router sends an APS Update Device command (packet #91) to the trust center to inform it whether a node has joined or left the network. The following table and Figure 5-15 provide details about the update status of the device, from which the trust center takes necessary action, which is to send the network or remove the key and associated security counters for the device.
Figure 5-14. Tunneling
The trust center sends the APS tunnel command frame in packet #93. The tunnel command frame contains the secured frame to be sent to the destination in its payload. Packet #95 shows the APS Transport Key command frame sent from the router parent to the newly joined end-device. It includes the key sequence number and the active network key. In case the router joins with a pre-configured network key, the APS transport packet contains a key sequence number and the key values as all-zeros. The end-device receives the Transport Key command frame, sets and activates the network key and does a device announcement to the network (packets #97 and #98).
Table 5-1. Status Field in APS Update Device Command
Parameter NameTypeValid RangeDescription
StatusInteger0x00-0x07Indicates the updated status of the device given by the DeviceAddress parameter.
  • 0x00 = Standard device secured rejoin
  • 0x01 = Standard device unsecured join
  • 0x02 = Device left
  • 0x03 = Standard device unsecured rejoin
  • 0x04 = High security device secured rejoin
  • 0x05 = High security device unsecured join
  • 0x06 = Reserved
  • 0x07 = High security device unsecured rejoin
Note: For more details on the status field in APS update device command, refer to the ZigBee Specification Revision 22 1.0 (05-3474-22).
Figure 5-15. Update Device Status