31.5.2.13 Interrupt Status and Interrupts Arbitration
The Interrupt Status register stores all channels with pending interrupts, as illustrated in the following figure.
The Event System can arbitrate between all channels with pending interrupts. The arbiter can be configured to prioritize statically or dynamically the incoming events. The priority is evaluated each time a new channel has an interrupt pending or an interrupt is cleared. The Channel Pending Interrupt register (INTPEND) provides the channel number with the highest interrupt priority, the corresponding channel interrupt flags and status bits.
By default, static arbitration is enabled (PRICTRL.RREN is ‘0’), the arbiter will prioritize a low channel number over a high channel number as illustrated in Figure 31-3. When using the status scheme, there is a risk of high channel numbers never being granted access by the arbiter. This can be avoided using a dynamic arbitration scheme.
The dynamic arbitration scheme available in the Event System is round-robin. Round-robin arbitration is enabled by writing PRICTRL.RREN to one. With the round-robin scheme, the channel number of the last channel being granted access will have the lowest priority the next time the arbiter has to grant access to a channel, as illustrated in the following figure. The channel number of the last channel being granted access, will be stored in the Channel Priority Number bit group in the Priority Control register (PRICTRL.PRI).
The Channel Pending Interrupt register (INTPEND) also offers the possibility to indirectly clear the interrupt flags of a specific channel. Writing a flag to one in this register, clears the corresponding interrupt flag of the channel specified by the INTPEND.ID bits.