7 Making a 3.3V Board

7.1 Overview

A 3.3V board is a hardware configuration in which both the Nano Debugger and the target device operate at the same fixed voltage of 3.3V.

The following block diagram illustrates the components of a 3.3V board configuration.

The USB-C connector supplies power to a fixed 3.3V regulator, which in turn powers both the Nano Debugger and the target MCU.

7.2 Hardware Design Procedure

Start your design process by consulting the schematic relevant to your board type. This schematic is provided as a PDF in the Appendix and is also available as an Altium project.

Review the detailed hardware description provided in this chapter. For each component within each subsystem, you may take one of the following actions:

  • Use the exact component specified, or an alternative package variant of that component. These components are strongly recommended and have been validated by Microchip.
  • Use a similar component, ensuring that its characteristics meet the requirements specified for the original component in the component lists. For active components, such as level shifters, the control pin functionality must be identical. Note that substituting a recommended component with an alternative may introduce risk to your design. Passive components are not fully specified and must comply with the ratings and grades indicated in the component tables.
  • You may choose to omit the component entirely. However, components such as USB filtering and protection are important for meeting certification requirements in certain regions. Omitting these components or making significant design changes is done at your own risk and may impact product compliance and reliability.
:

The components specified in the reference schematic have been chosen to meet the temperature range of -40°C to +85°C.

Fastpath:

For passive components such as resistors and capacitors, manufacturer part numbers (MPNs) are not provided. You may source these components according to your preferences, as long as they meet the specified ratings and ranges.

7.2.1 Common Hardware Description

This section applies to all board types that utilize the Nano Debugger.

USB Related

The Nano Debugger utilizes a SAMD21 microcontroller and functions as a USB full-speed device, supporting bit rates up to 12 Mb/s. A USB Type-C connector is recommended for optimal compatibility and performance, although other connector types may be considered based on specific design requirements.

A USB-C downstream device (sink) must connect both Configuration Channel lines (CC1 and CC2) to ground using 5.1kΩ resistors, while leaving the Sideband Use lines (SB1 and SB2) unconnected. For enhanced protection, it is strongly recommended to include ESD suppression diodes to safeguard the Nano Debugger against electrostatic discharge events.

Table 7-1. USB Component List
FunctionDesignatorDescriptionManufacturer/MPNNotes
USB connectorJ100USB 2.0 type C receptacleGCT USB4105-GF-AAny suitable USB connector can be used as an alternative
CC1, CC2 line controlR1085.1k, 1%-Mandatory for USB-C
R1095.1k, 1%-
ESD protection of the USB data linesD101ESD suppressorLittelfuse PGB1010402KRRecommended for product certification
D102ESD suppressorLittelfuse PGB1010402KR

Power Supply

Multiple conditioning stages are necessary to operate the Nano Debugger at 3.3V, which is supplied from the USB VBUS.

  1. USB VBUS typically ranges from 4.4V to 5.5V. When a USB cable is connected to the board, transient voltage events—such as voltage spikes from capacitive charging, inrush currents, and potential ESD pulses—can occur at the connector. These transients usually last from microseconds to milliseconds and may damage connected circuitry if not properly managed. The VBUS overvoltage protection circuit safeguards against voltages up to 20V and introduces a 4 ms startup delay. This combination protects the power supply from voltage spikes and provides the Nano Debugger with a soft start during connection.

  2. A current-limiting switch is implemented to protect the upstream computer and USB subsystem from overcurrent conditions that could damage the USB port or cause it to disconnect. This protection is particularly important in scenarios where end-users might connect peripheral hardware incorrectly, potentially resulting in excessive current draw—a frequent issue with development boards. The reference design's current limit can be adjusted by modifying the value of the associated resistor.
  3. A low dropout regulator (LDO) provides a stable 3.3V output by regulating the protected and filtered VBUS signal.
  4. USB overvoltage protection is strongly recommended, particularly for USB‑powered development kits, where boards may be exposed to ground loops caused by connecting oscilloscope probes. Such ground loops can be destructive to the power supply.
Table 7-2. Power Supply Component List
FunctionDesignatorDescriptionManufacturer/MPNNotes
USB overvoltage protectionU101USB Positive Overvoltage Protection ControllerOnSemi NCP360SNAET1GHighly recommended
C1002.2 µF, 16V-
C1014.7 µF, 16V-
VBUS current limitingU102Adjustable current‑limiting power distribution switchMicrochip MIC2009ALimits current to 507 mA - 877 mA
R100300R, 1%-
C1034.7 µF, 16V-
LDO regulatorU103Low quiescent current LDOMicrochip MCP1755/3.3VAny suitable 3.3V regulator with high VIN tolerance can be used (for example, the MCP1755 has a 16V maximum VIN )
C1014.7 µF, 16V-

Nano Debugger MCU

The Nano Debugger utilizes a Microchip SAMD21 microcontroller. Use the components specified in this documentation or adhere to the recommended design guidelines for the SAMD21 MCU.

Table 7-3. MCU Component List
FunctionDesignatorDescriptionManufacturer/MPNNotes
Debugger MCUU100Nano DebuggerMicrochip ATSAMD21E18A-AUT
Decoupling capacitorsC1040.1 µF, 16V-Mandatory decoupling capacitors for the MCU and core
C1050.1 µF, 16V-
C1061 µF, 16V-
Programming interfaceJ1041.27 mm (50 mil) 2x520021111-00010T4LFAny suitable connector mechanism can be used to program the MCU

Miscellaneous

Additional subsystems utilized by the Nano Debugger include:

  • The Nano Debugger measures the target voltage using an ADC. A resistor divider is implemented to scale down the target voltage, which may exceed 3.3V, to a safe level for the ADC input. The resistor values are carefully selected to minimize current draw while ensuring the sampling capacitor charges properly. Using lower resistor values could risk current flowing into the Nano Debugger’s I/O pins if the target voltage is present while the Nano Debugger is unpowered.

  • The Nano Debugger uses a single LED in an active-low configuration to indicate its status to end users. If a different LED is selected, the series resistor value can be adjusted to modify the LED brightness as needed.

  • In the unlikely event of faulty debugger firmware, end users can short the BOOT jumper during power-up. This action forces the Nano Debugger into upgrade mode, enabling users to recover the device.

Table 7-4. Miscellaneous Component List
FunctionDesignatorDescriptionManufacturer/MPNNotes
VBUS samplingR10147k, 1%-Mandatory. Enables the debugger to sample VBUS.
R10247k, 1%-
Target voltage samplingR1031M, 1%-Mandatory. Enables the debugger to sample target voltage.
R1041M, 1%-
Status LEDD100LEDStanley VFHL1111C-4B23C-TRRecommended for user feedback
R1101k, 1%-
Boot jumperTP100pad/jumper-Mandatory - pad/jumper between PA27 of the MCU and GND for recovery
TP101pad/jumper-

7.2.2 Specific Hardware Description

Important: This section is incomplete and not ready for use

7.3 Default Firmware Image

When using the default firmware image, the board configuration provides the feature set listed below. If you want to create a 3.3V board with additional features enabled, a manufacturing configuration is required. See Optional: Debugger Configuration.

Table 7-5. Default Configuration
FeatureDefault
Programming/Debug InterfacesArm SWD
DeviceUnspecified default device (blank)
Power

No level shifters are included.

No adjustable regulator is present (the debugger cannot adjust the target voltage).

Target voltage measurement is supported (the debugger can measure the target voltage).
VoltageOperating range: 3.0V to 3.6V
Serial numberAutomatic USB serial number generation
Auxiliary interfaces

Virtual Serial Port/CDC.

One DGI GPIO channel (GPIO0).

No ID SYSTEM channel.

Kit name stringMicrochip Nano Debugger kit
Manufacturer name stringMicrochip