1.2.4 Device Revision
The package marking on Microchip security devices does not identify the
device type. Therefore, the package marking cannot be used to identify the ATECC608B device. The only way to identify the device is
through use of the device revision. The hardware device revision can be read by using
the Revision mode (0x00) of the
Info command. The output response of
the Info command for each device is as follows:Note:
- The value of the fourth byte may change over time, but it is 0x03 at the time of the initial product release.
- The value of the Revision mode response is not the same as the 4-byte RevNum (Bytes[4:7]) in the device configuration zone. Only the Revision mode response can be used for device identification.