2.6.4 USR_MLME_AssociateInd callback Function
C
void USR_MLME_AssociateInd(uint64_t DeviceAddress, uint8_t CapabilityInformation)Summary
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.indication.
Description
This function implemented by application (NHLE) for MAC service MLME-ASSOCIATE.indication.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| DeviceAddress | Extended address of device requesting association |
| CapabilityInformation | Capabilities of device requesting association. (@ref WPAN_CAP_ALTPANCOORD |
Returns
None.
Example
void USR_MLME_AssociateInd(uint64_t DeviceAddress, uint8_t CapabilityInformation)
{
DeviceAddress = DeviceAddress;
CapabilityInformation = CapabilityInformation;
}Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.