2.6.3 WPAN_MLME_AssociateResp Function
C
bool WPAN_MLME_AssociateResp(uint64_t DeviceAddress, uint16_t AssocShortAddress,uint8_t status)Summary
Initiate MLME-ASSOCIATE.response service and place it in the MLME-SAP queue.
Description
This function is used to send the associate response on the receipt of Associate Indication from MAC layer. It initiates MLME-ASSOCIATE.response service and place it in the MLME-SAP queue. The MLME-ASSOCIATE.response primitive is used to initiate a response to an MLMEASSOCIATE.indication primitive.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| DeviceAddress | Extended address for device requesting association |
| AssocShortAddress | Short address allocated on successful association |
| status | Status of the association attempt. Valid values:- @ref ASSOCIATION_SUCCESSFUL, PAN_AT_CAPACITY, PAN_ACCESS_DENIED, ASSOCIATION_RESERVED |
Returns
true - success; false - buffer not available or queue full.
Example
usr_mlme_associate_ind_t *mlmeAssocInd; usr_mlme_associate_ind_t assocInd; assocInd.CapabilityInformation = mlmeAssocInd->CapabilityInformation; assocInd.DeviceAddress = mlmeAssocInd->DeviceAddress; uint16_t associate_short_addr = 0x0001U; bool retVal = false; retVal = WPAN_MLME_AssociateResp(assocInd.DeviceAddress, associate_short_addr, ASSOCIATION_SUCCESSFUL); if (true != retVal) { printf("buffer not available or queue full"); }
Remarks
On the receipt of WPAN_MLME_AssociationResp, MAC layer will perform respective operation and asynchronously invokes USR_MLME_AssociateInd with proper status.