2.3.1 WPAN_MLME_SetReq Function
C
bool WPAN_MLME_SetReq(uint8_t PIBAttribute, void *PIBAttributeValue)Summary
Initiate MLME-SET.request service and have it placed in MLME_SAP queue.
Description
This function is used to write the given value to the indicated PIB attribute Initiate MLME-SET.request service and have it placed in MLME_SAP queue. MLME-SAP set primitives define how PIB attributes may be written.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| PIBAttribute | PIB attribute to be set |
| PIBAttributeValue | Pointer to new PIB attribute value |
Returns
true - success; false - buffer not available or queue full.
Example
bool retVal = false; uint8_t beacon_payload_len = 20; retVal = WPAN_MLME_SetReq(macBeaconPayloadLength, &beacon_payload_len); if (true != retVal) { printf("buffer not available or queue full"); }
Remarks
On the receipt of WPAN_MLME_SetReq, MAC layer will perform respective operation and asynchronously invokes USR_MLME_SetConf with proper status.