2.3.4 USR_MLME_GetConf callback Function
C
void USR_MLME_GetConf(uint8_t status,uint8_t PIBAttribute, void *PIBAttributeValue)Summary
Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm.
Description
This function implemented by application (NHLE) for MAC service MLME-GET.confirm.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| status | Result of requested PIB attribute get operation |
| PIBAttribute | Retrieved PIB attribute |
| PIBAttributeValue | Pointer to data containing retrieved PIB attribute |
Returns
None.
Example
void USR_MLME_GetConf(uint8_t status,uint8_t PIBAttribute, void *PIBAttributeValue)
{
status = status;
PIBAttribute = PIBAttribute;
PIBAttributeValue = PIBAttributeValue;
}
Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.