4.3.2 Programming with the DediProg SF100

As described in 4.3.1 Programming with the DediProg SF600, the recommended method for programming the SPI NOR Flash chips on the EV42J24A is via the use of a DediProg SF600 level, in-system programmer. However, many users have only an SF100 level programmer available, and the previous board for the CEC173x was only supported by the SF100. The SF100 programmer can be enabled to work with the EV42J24A by using a flywire connection, as shown below. Jumper wires can be easily attached between pins on the programmer and the EV42J24A.

Figure 4-4. Programming the EV42J24A using the SF100 programmer and Flywire connections

The details of this connection are shown in the figure below. The basic programming procedure remains the same, and it is recommended to set the jumpers to obtain power from the programmer. Unlike the SF600, the SF100 supplies only a single chip select. Therefore, to program both SPI chips with the SF100, the user must manually move the chip select wire between chip select pins on the header, as indicated below. To program all four devices, the SF100 must first be connected to header J61, which connects to SPI Channel 0, and the chip select signal must be sequentially connected between CS1 and CS2. Then, this procedure must be repeated by connecting the SF100 to header J62, which connects to SPI Channel 1 and the respective chip selects.

Figure 4-5. SF100 programmer to CEC1736 Programming Header Flywire connections

Alternatively, DediProg supplies the ISP-SP-CB flywire cable. Using this cable and a 2x6 header socket, it is easy to make a simple programming cable.

Figure 4-6. DediProg ISP-SP-CB Flywire cable

The DediProg ISP-SP-CB 10-pin Split Cable has a 14-pin header (only 10 of the pins are used for the ISP Split Cable), which can be connected directly to the SF100 ISP header. Each individual split cable has a different color and is labeled with the pin name for easy identification.

Shown below is a complete programming log using the SF100 programmer and the flywire setup. Note that this setup supports single I/O only, but programs at 24 MHz. These settings come from the miscellaneous section under the config button.

Figure 4-7. Programming Log with SF100 Programmer