3.1.1 Modifiable Configuration Zone Bytes
No bytes within the Configuration Zone can be directly written because the Config Zone is already locked. Several bytes can still be modified through the use of other commands.
SlotLocked Bits
For the ATECC608C-TFLXTLS, the
following individual slots may be uniquely configured to be
slot lockable or not: Slots 2-6, 8, 10-12, 13 and
15. Through
use of the Trust Platform Design Suite tools, each of these slots may be set to
either be fixed or locked at time of manufacturing. Slots 10-12 must always be set
the same way. If set to be lockable the SlotLock mode of the Lock
command can be used to lock a given slot. Each slot where this feature is enabled
can be individually locked just once. Once a slot has been locked, it can never be
modified or unlocked but can still be used based on the Access Policies defined for
that slot.
Bytes 88 and 89 store the SlotLocked bytes. Initially, all bits in these bytes are set to a value of one. For those slots that have been locked, the value of the respective bit will be set to a value of zero.
I2C Address Redefinition
UpdateExtra command can be
used to rewrite byte 85 of the Configuration zone to a new I2C address.
When this byte is set to a non-zero value, the device configuration uses byte 85 as
its I2C address instead of the default address. Once this byte has been
rewritten, the device must be powered-down or put into Sleep mode before this change
takes effect.User Extra Byte
The UserExtra byte can be used for any desired purpose. This byte can be
updated just once with the UpdateExtra command. The UserExtra byte
is located at byte 84 of the Configuration zone.
Counter[0,1]
While the counters are not used by this device, they are not disabled. If so desired, the monotonic counters may be used by the system. Note that the counters are initialized to zero and can count to the maximum value of 2,097,151. The counter value can be incremented or read through the use of theCounter
command. How this counter is used is strictly up to the system and independent of
anything else on the device. Counter values can be read or updated using the
Counter command.