4.2.1 Setup
The M-HSM Control Panel application is located in the "M-HSMControlPanel" folder.
The application executable M-HSMControlPanel.exe can be started like other Windows applications and does not require admin privileges to operate.
For convenience, it can be added to the Windows start-up applications as a shortcut placed in the the Windows Startup folder:
For example, C:\Users\hsm_nonAdmin_user\AppData\Roaming\Microsoft\Windows\Start Menu\Programs\Startup
Once added to the startup applications, the M-HSM Control Panel application is automatically started by the Windows upon startup.
Only one running instance of the application is allowed at a time.