4.2.2 Notification Icon
The application appears as an icon in the Windows Notification Area.
![]()
Depending on the status of the M-HSM server, the icon of the M-HSM Control Panel application can be one of the following:
- Green: Indicates server normal working state.
- Red: Indicates that the connection with the server is established, but the session with the HSM module is not active. It can be either in the Starting, Stopping, or Not Running state.
- Gray: Indicates connection with the server cannot be established. In most cases, this means that the service is not running.
In addition to color coding, the server state is indicated in the tooltip that appears when the cursor hovers over the icon.
The following figure shows how left-clicking the application icon opens the context menu: