53.7.4 Calculating the Correct Crystal Decoupling Capacitor
The model shown in Figure 53-11 can be used to calculate correct load capacitor for a given crystal. This model includes internal capacitors CLn, external parasitic capacitance CELn and external load capacitance CPn.
Using this model, the total capacitive load for the crystal can be calculated as shown in the equation below:
where:
Ctot is the total load capacitance seen by the crystal. This value must be equal to the load capacitance value found in the crystal data sheet.
The parasitic capacitance CELn can be in most applications be disregarded as these are usually very small. If accounted for, these values are dependent on the PCB material and PCB layout.
For some crystal, the internal capacitive load provided by the device itself can be enough. To calculate the total load capacitance in this case. CELn and CPn are both zero, CL1 = CL2 = CL, and the equation reduces to the following:
For equivalent internal pin capacitance values, refer to the section Crystal Oscillator Characteristics.