19.7.1 Block Transfer Control

The BTCTRL register offset is relative to (BASEADDR or WRBADDR) + Channel Number * 0x10.
Name: BTCTRL
Offset: 0x00
Reset: 0x0000
Property: –

Bit 15141312111098 
 STEPSIZE[2:0]STEPSELDSTINCSRCINCBEATSIZE[1:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 76543210 
    BLOCKACT[1:0]EVOSEL[1:0]VALID 
Access R/WR/WR/WR/WR/W 
Reset 00000 

Bits 15:13 – STEPSIZE[2:0] Address Increment Step Size

This bit field selects the step size of the address increment. The setting applies to the to source or destination address, depending on the STEPSEL setting.

ValueNameDescription
0x0 X1 Next ADDR = ADDR + (Beat size in byte) * 1
0x1 X2 Next ADDR = ADDR + (Beat size in byte) * 2
0x2 X4 Next ADDR = ADDR + (Beat size in byte) * 4
0x3 X8 Next ADDR = ADDR + (Beat size in byte) * 8
0x4 X16 Next ADDR = ADDR + (Beat size in byte) * 16
0x5 X32 Next ADDR = ADDR + (Beat size in byte) * 32
0x6 X64 Next ADDR = ADDR + (Beat size in byte) * 64
0x7 X128 Next ADDR = ADDR + (Beat size in byte) * 128

Bit 12 – STEPSEL Step Selection

This bit controls if the source or destination addresses are using the step size settings.

ValueNameDescription
0x0 DST Step size settings apply to the destination address
0x1 SRC Step size settings apply to the source address

Bit 11 – DSTINC Destination Address Increment Enable

This bit controls whether the destination address increments between beat transfers or not. When this bit is set, the destination address is by default incremented by one beat size in byte(s). If the STEPSEL bit is ‘0’, the STEPSIZE register will control the size of the increments.

ValueDescription
0 The destination address increment is disabled
1 The destination address increment is enabled

Bit 10 – SRCINC Source Address Increment Enable

This bit controls whether the source address increments between beat transfers or not. When this bit is set, the source address is by default incremented by one beat size in byte(s). If the STEPSEL bit is ‘1’, the STEPSIZE register will control the size of the increments.

ValueDescription
0 The source address increment is disabled
1 The source address increment is enabled

Bits 9:8 – BEATSIZE[1:0] Beat Size

This bit field controls the size of one beat. A beat is the size of one data transfer bus access, and the setting applies to both read and write accesses.

ValueNameDescription
0x0 BYTE 8-bit
0x1 HWORD 16-bit
0x2 WORD 32-bit
Other — Reserved

Bits 4:3 – BLOCKACT[1:0] Block Action

This bit field controls what actions the DMAC will take after a block transfer has completed.

ValueNameDescription
0x0 NOACT Channel will be disabled if it is the last block transfer in the transaction
0x1 INT Channel will be disabled if it is the last block transfer in the transaction and block interrupt
0x2 SUSPEND Channel suspend operation is completed
0x3 BOTH Both channel suspend operation and block interrupt

Bits 2:1 – EVOSEL[1:0] Event Output Selection

This bit field controls the event output selection.

ValueNameDescription
0x0 DISABLE Event generation disabled
0x1 BLOCK Event strobe when block transfer complete
0x2 — Reserved
0x3 BEAT Event strobe when beat transfer complete

Bit 0 – VALID Descriptor Valid

Writing a ‘0’ to this bit in the Descriptor or Write-Back memory will suspend the DMA channel operation when fetching the corresponding descriptor.

The bit is automatically cleared in the Write-Back memory section when the channel is aborted, when an error is detected during the block transfer, or when the block transfer is completed.

ValueDescription
0 The descriptor is not valid
1 The descriptor is valid