7.2 Port List
(Ask a Question)The following tables list the User Cryptoprocessor port list for the PolarFire family.
| Port Name | Direction | Description |
|---|---|---|
| AHB_SLAVE | Bus | AHB-Lite slave interface, which is used for control, and primary data input and output. |
| AHB_MASTER | Bus | AHB-Lite master DMA interface, which may optionally be used for data input and output. |
| DRI_SLAVE | Bus | Control and status signals are accessible through the DRI. |
| HCLK | Input | AHB bus clock. |
| HRESETN | Input | The reset signal, CRYPTO_HRESETN, is active low, synchronous, and is sampled on the rising edge of the clock. Asserts the functional reset of the User Cryptoprocessor block and zeroizes all the internal RAM and registers as PURGE signal. It is necessary to assert this signal for a minimum of two clock cycles to reset the core. |
| START | Input | External execution initiation input when the User Cryptoprocessor operates in the standalone configuration without a host processor connected to the bus interface. Asserting the START signal causes the User Cryptoprocessor to initiate execution. During execution, the status of the User Cryptoprocessor is reflected by the BUSY and DLL_LOCK ports. This signal must be tied low when the User Cryptoprocessor is used as a co-processor. |
| PURGE | Input | When the signal is set to '1', it initializes the Zeroization of User
Cryptoprocessor internal RAM and registers. For normal operation, this
signal must be tied low. The PURGE input is level sensitive, and if the
PURGE pin is still asserted when a purge operation completes, another
purge operation is initiated. Note: In PolarFire
devices, the PF_DRI macro can be used from the fabric to exercise
the PURGE functionality of the User Cryptoprocessor. It is important
to note that once the data is purged, it cannot be recovered, so it
is essential to use this functionality with caution. |
| STALL | Input | Stalls the User Cryptoprocessor for a clock cycle, to introduce variance in the external signatures. The STALL input is expected to be generated by a LFSR circuit in the fabric and asserted randomly for a single cycle to achieve the required stall rates. The STALL input must not be asserted until at least three clock cycles after the HRESETN is de-asserted and the DLL has indicated LOCK for three cycles. |
| ALARM | Output | Asserted to indicate an uncorrectable memory error condition. An uncorrectable memory error causes the Crypto core to perform a reset and purge. This reset terminates any in-progress operation. For most CAL operations, the CALPKTrfRes() function is used to complete the operation and generates a hardware fault code in the event of an alarm. |
| BUS_ERROR | Output | Asserted when a HRESP response error is detected by the User Cryptoprocessor AHB master. When set, a reset is required to clear. |
| BUSY | Output | Execution status signal |
| COMPLETE | Output | Active high signal, asserted on raising edge of CRYPTO_HCLK to indicate that the User Cryptoprocessor has completed an operation. This signal can be connected to the host microprocessor as an interrupt request signal, enabling the User Cryptoprocessor to interrupt the processor when it completes an operation. |
| DLL_LOCK | Output | DLL lock status |
Important: In PolarFire FPGA and RT PolarFire FPGA
devices, the User Crypto processor's control and status registers are accessible to the
user logic through DRI interface. See PolarFire Device Register Map for more
information about the User Crypto registers.
| Port Name | Direction | Description |
|---|---|---|
| CRYPTO_AHB_SLAVE | Bus | AHB-Lite slave interface, which is used for control, and primary data input and output. |
| CRYPTO_AHB_MASTER | Bus | AHB-Lite master DMA interface, which may optionally be used for data input and output. |
| CRYPTO_HCLK | Input | AHB bus clock. |
| CRYPTO_HRESETN | Input | The reset signal, CRYPTO_HRESETN, is active low, synchronous, and is sampled on the rising edge of the clock. Asserts the functional reset of the User Cryptoprocessor block and zeroizes all the internal RAM and registers as PURGE signal. It is necessary to assert this signal for a minimum of two clock cycles to reset the core. |
| CRYPTO_GO_F2M | Input | External execution initiation input when the User Cryptoprocessor operates in the standalone configuration without a host processor connected to the bus interface. Asserting the GO signal causes the User Cryptoprocessor to initiate execution. During execution, the status of the User Cryptoprocessor is reflected by the BUSY and DLL_LOCK ports. This signal must be tied low when the User Cryptoprocessor is used as a co-processor. |
| CRYPTO_PURGE_F2M | Input | When the signal is set to '1', it initializes the Zeroization of User Cryptoprocessor internal RAM and registers. For normal operation, this signal must be tied low. The PURGE input is level sensitive, and if the PURGE pin is still asserted when a purge operation completes, another purge operation is initiated. |
| CRYPTO_STALL_F2M | Input | Stalls the User Cryptoprocessor for a clock cycle, to introduce variance in the external signatures. The STALL input is expected to be generated by a LFSR circuit in the fabric and asserted randomly for a single cycle to achieve the required stall rates. The STALL input must not be asserted until at least three clock cycles after the HRESETN is de-asserted and the DLL has indicated LOCK for three cycles. |
| CRYPTO_ALARM_M2F | Output | Asserted to indicate an uncorrectable memory error condition. An uncorrectable memory error causes the Crypto core to perform a reset and purge. This reset terminates any in-progress operation. For most CAL operations, the CALPKTrfRes() function is used to complete the operation and generates a hardware fault code in the event of an alarm. |
| CRYPTO_BUSERROR_M2F | Output | Asserted when a HRESP response error is detected by the User Cryptoprocessor AHB master. When set, a reset is required to clear. |
| CRYPTO_BUSY_M2F | Output | Execution status signal |
| CRYPTO_COMPLETE_M2F | Output | Active high signal, asserted on raising edge of CRYPTO_HCLK to indicate that the User Cryptoprocessor has completed an operation. This signal can be connected to the host microprocessor as an interrupt request signal, enabling the User Cryptoprocessor to interrupt the processor when it completes an operation. |
| CRYPTO_DLL_LOCK_M2F | Output | DLL lock status |
| CRYPTO_MESH_CLEAR_F2M | Input | Crypto Mesh error clear should be asserted for at least 5 ns |
| CRYPTO_MESH_ERROR_M2F | Output | Indicates that the security mesh detected an error because of wires are cut or shorted. When set, stays set until cleared. |
| Cryptoprocessor Ownership Handshake Interface | ||
| CRYPTO_REQUEST_F2M | Input | Fabric request or is using the Cryptoprocessor |
| CRYPTO_MSS_REQUEST_M2F | Output | MSS request or is using the Cryptoprocessor |
| CRYPTO_RELEASE_F2M | Input | Fabric released the Cryptoprocessor |
| CRYPTO_MSS_RELEASE_M2F | Output | MSS released the Cryptoprocessor |
| CRYPTO_OWNER_M2F | Output | Indicates that the Fabric owns the Cryptoprocessor and the fabric interface is enabled |
| CRYPTO_MSS_OWNER_M2F | Output | Indicates that the MSS owns the Cryptoprocessor and the fabric interface is disabled |
| CRYPTO_REQUEST_F2M | Input | Fabric request or is using the Cryptoprocessor |
| CRYPTO_MSS_REQUEST_M2F | Output | MSS request or is using the Cryptoprocessor |
| Cryptoprocessor Streaming Interface | ||
| CRYPTO_XWDATA_F2M | Input | Transfer in data |
| CRYPTO_XWADDR_M2F | Output | Transfer in data address output |
| CRYPTO_XENABLE_F2M | Input | Transfer in data request |
| CRYPTO_XINACCEPT_M2F | Output | Transfer in data accept |
| CRYPTO_XRDATA_M2F | Output | Transfer out data |
| CRYPTO_XRADDR_M2F | Output | Transfer out data address output |
| CRYPTO_XVALIDOUT_M2F | Output | Transfer out data valid output |
| CRYPTO_XOUTACK_F2M | Input | Transfer out data acknowledgment |
Note: 1. Input refers to an input port to MSS from Fabric and output refers to an output port from MSS to Fabric.