4.5.1 Execution
main.c - Initialize the socket and get the time from the NTP server.
- Code summary.
- Configure the network
parameters in main.h.
/** Wi-Fi Settings */ #define MAIN_WLAN_SSID "DEMO_AP" /**< Destination SSID */ #define MAIN_WLAN_AUTH M2M_WIFI_SEC_WPA_PSK /**< Security manner */ #define MAIN_WLAN_PSK "12345678" /**< Password for Destination SSID */ - Initialize the socket
module and register the socket callback function.
/* Initialize Socket module */ socketInit(); /* Register socket handler, resolve handler */ registerSocketCallback(socket_cb, resolve_cb); - Connect to the AP.
/* Connect to router. */ m2m_wifi_connect((char *)MAIN_WLAN_SSID, sizeof(MAIN_WLAN_SSID), MAIN_WLAN_AUTH, (char *)MAIN_WLAN_PSK, M2M_WIFI_CH_ALL); - After the device is
connected to the AP, create a UDP socket and bind it in the main loop.
if (udp_socket < 0) { udp_socket = socket(AF_INET, SOCK_DGRAM, 0); if (udp_socket < 0) { printf("main: UDP Client Socket Creation Failed.\r\n"); continue; } /* Initialize default socket address structure. */ addr_in.sin_family = AF_INET; addr_in.sin_addr.s_addr = _htonl(MAIN_DEFAULT_ADDRESS); addr_in.sin_port = _htons(MAIN_DEFAULT_PORT); bind(udp_socket, (struct sockaddr *)&addr_in, sizeof(struct sockaddr_in)); - Initialize the socket
module and send an NTP time query to the NTP server in the
resolve_cb()
function
static void resolve_cb(uint8_t *pu8DomainName, uint32_t u32ServerIP) { ... if (udp_socket >= 0) { addr.sin_family = AF_INET; addr.sin_port = _htons(MAIN_SERVER_PORT_FOR_UDP); addr.sin_addr.s_addr = u32ServerIP; ret = sendto(udp_socket, (int8_t *)&cDataBuf, ...); } - Receive the NTP time from
the server and convert it in the socket_cb()
function.
static void resolve_cb(uint8_t *pu8DomainName, uint32_t u32ServerIP) { ... if (udp_socket >= 0) { addr.sin_family = AF_INET; addr.sin_port = _htons(MAIN_SERVER_PORT_FOR_UDP); addr.sin_addr.s_addr = u32ServerIP; ret = sendto(udp_socket, (int8_t *)&cDataBuf, ...); } - Parse the time from the
received server
response.
static void socket_cb(SOCKET sock, uint8_t u8Msg, void *pvMsg) { ... case SOCKET_MSG_RECVFROM: { /* printf("socket_cb: socket_msg_recvfrom!\r\n"); */ tstrSocketRecvMsg *pstrRx = (tstrSocketRecvMsg *)pvMsg; if (pstrRx->pu8Buffer && pstrRx->s16BufferSize) { uint8_t packetBuffer[48]; memcpy(&packetBuffer, pstrRx->pu8Buffer, sizeof(packetBuffer)); ... uint32_t secsSince1900 = packetBuffer[40] << 24 | packetBuffer[41] << 16 | packetBuffer[42] << 8 | packetBuffer[43]; /* Now convert NTP time into everyday time. * Unix time starts on Jan 1 1970. In seconds, that's 2208988800. * Subtract seventy years. */ const uint32_t seventyYears = 2208988800UL; uint32_t epoch = secsSince1900 - seventyYears; /* Print the hour, minute and second. GMT is the time at Greenwich Meridian. */ printf("socket_cb: The GMT time is %lu:%02lu:%02lu\r\n", (epoch % 86400L) / 3600, /* hour (86400 equals secs per day) */ (epoch % 3600) / 60, /* minute (3600 equals secs per minute) */ epoch % 60); /* second */
- Configure the network
parameters in main.h.
- Build the program and download it into the board.
- Start the application.