7.1.1 Auto Board Identification of Xplained Mini Kit
- Once the ATmega328PB Xplained Mini
kit is connected to the PC, the Windows® Task bar
will pop-up a message as shown below:
Figure 7-1. ATmega328PB Xplained Mini Driver Installation
- If the driver installation is proper,
EDBG will be listed in the Device Manager as shown below:
Figure 7-2. Successful mEDBG Driver Installation
-
Open Atmel Studio and go to View → Available Tools. The EDBG should get listed in the tools as mEDBG and the tool status should display as Connected. This indicates that the tool is communicating properly with Atmel Studio.
Figure 7-3. mEDBG under Available Tools