7.1.2 Connect the ATmega328PB Xplained Mini UART to the mEDBG COM Port
- Connect the mEDBG USB to the PC.
- Use the Device Manager to find the COM port number.
- Default COM port settings are 9600 baud N 8 1. The COM port settings can be changed according to the application by using the Device Manager. This application has been tested with a baud rate of 115200.