3.3.3 Debugger Adapter Board

For legacy connections, the Debugger Adapter Board (AC102015) is available.

The MPLAB PICkit Basic can be connected to the Debugger Adapter Board as shown in the sections below. Then the various connections on the adapter board can be used to connect to specific targets (refer to the following section).

Alternatively the AVR Programming Adapter Board (AC31S18A) is available for use with MPLAB PICkit 5, PICkit 4, PICkit Basic and Snap.

Using the 8-pin Inline Connector

Using the Single In-Line (SIL) connector, the tool is connected directly to the adapter board (ensure pin 1 on the tool lines up with pin 1 on the adapter board). If a 6-pin SIL header is used, connections 7 (TMS) and 8 (TDI) will not be available.

Figure 3-6. SIL Connection at Debugger Adapter Board

Using the 8-pin Modular Connector

For the MPLAB PICkit Basic it is recommended that you use the 8-pin inline connector described above.

Using the AC164110 - RJ-11 to ICSP Adapter, the debugger can be connected to the modular connector using a 6-pin modular cable resulting in the loss of connection to pins 8 (TMS) and 1 (TDI) at the adapter board.

Figure 3-7. RJ-45 at the Debugger Adapter Board