3.4 Diagnostics Status Notification
The DiagnosticsStatusNotification message in OCPP 1.6J reports the status of diagnostic log uploads from the charge point to the central system, such as "Uploading”, "Uploaded" or "UploadFailed". It helps track the progress and success of diagnostic data transfers.
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
OCPPDiagnosticStatusNotificationResetGlobals | Function to reset global variables for Diagnostic Status Notification. | void | DIAGNOSTIC_STATUS_NOTIFICATION_STATE_T |
Example:
void OCPPResetAllGlobals(void)
{
UtilitiesGlobalVariablesReset();
UtilitiesLocalStorageResetGlobals();
OCPPSetChargingProfileResetGlobals();
OCPPGetCompositeScheduleResetGlobals();
CPPClearChargingProfileResetGlobals();
OCPPReserveNowResetGlobals();
OCPPCancelReservationResetGlobals();
OCPPTriggerMessageResetGlobals();
OCPPSendLocalListResetGlobals();
OCPPGetLocalListVersionResetGlobals();
OCPPUpdateFirmwareResetGlobals();
OCPPGetDiagnosticsResetGlobals();
OCPPFirmwareStatusNotificationResetGlobals();
OCPPDiagnosticStatusNotificationResetGlobals();
OCPPUnlockConnectorResetGlobals();
OCPPStopTransactionResetGlobals();
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SendDiagnosticStatusNotificationRequest | This function sends a diagnostic status notification request to the server. It creates an OCPP frame for the request and sends it using sendframe. | void | DIAGNOSTIC_STATUS_NOTIFICATION_STATE_T |
Example:
case TRIGGER_MESSAGE_TYPE_DIAGNOSTICS_STATUS_NOTIFICATION:
SendDiagnosticStatusNotificationRequest();
break;
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SetChargerDiagnosticsInfo | This function sets the diagnostic information of the charger to Idle state. | status | void |
Example:
case 'd': /*DiagnosticsStatusNotification*/
{
uint8_t diagState = DIAGNOSTICSTATUSNOTIFICATION_IDLE; /*Idle State*/
LogDebug("APP_LOG", "Select the Diagnostic State\n\t0. Idle \n\t1. Uploaded\n\t2. UploadFailed\n\t3. Uploading \n\r");
result = scanf("%hhd",(char *)&diagState);
if (result != 1)
{
LogDebug("APP_LOG", "Error reading DiagState\n");
}
if (diagState < 4U)
{
SetChargerDiagnosticsInfo(diagState);
}
else
{
LogDebug("APP_LOG", "Selected the invalid Diagnostic State\n");
}
(void)SendDiagnosticStatusNotificationRequestS();
}
break;
case 'F': /*FirmwareStatusNotification*/
{
TestFirmwareStatusNotification();
}
break;
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
GetChargerDiagnosticNotificationStr | This function returns the status of DiagnosticStatusNotification in string format. | DIAGNOSTICSTATUSNOTIFICATION_T status | char* |
Example:
void GetChargerDiagnosticsInfo(char *str)
{
if (str == NULL)
{
/* Check for NULL pointer to avoid segmentation fault */
OCPPLogMessage(LOG_ERROR, LOG_SENDING, "Error: NULL parameter passed to get_charger_diagnostics_info\n\r");
return;
}
/* Copy the diagnostic information string to the provided destination string */
Safestrcpy(str, (char *)GetchargerDiagnosticNotificationStr(diagnosticStatusNotification.status), DIAGNOSTIC_STATUS_STRING_SIZE);
OCPPLogMessage(LOG_INFO, LOG_SENDING, " Get_charger_diagnostics_info: %s\n\r", str);
}
|
Syntax |
Description |
Constants/Members |
|---|---|---|
DIAGNOSTICSTATUSNOTIFICATION_T | Enum: Diagnostic status notification states | DIAGNOSTICSTATUSNOTIFICATION_IDLE DIAGNOSTICSTATUSNOTIFICATION_UPLOADED DIAGNOSTICSTATUSNOTIFICATION_UPLOAD_FAILED DIAGNOSTICSTATUSNOTIFICATION_UPLOADING |
DIAGNOSTIC_STATUS_NOTIFICATION_STATE_T | Enum: Diagnostic status notification error states | DIAGNOSTICSTATUSNOTIFICATION_SUCCESS DIAGNOSTICSTATUSNOTIFICATION_FAILED DIAGNOSTICSTATUSNOTIFICATION_RESPONSE_FAILED DIAGNOSTICSTATUSNOTIFICATION_RESPONSE_ACCEPT_FAILED DIAGNOSTICSTATUSNOTIFICATION_RESPONSE_SUCCESS |
RX_DIAGNOSTICSTATUSNOTIFICATION | DIAGNOSTICSTATUSNOTIFICATION_T status |