3.13 Change Configuration
The ChangeConfiguration message in OCPP 1.6J allows the central system to modify configuration settings on the charge point, such as communication or operational parameters. It includes the configuration key and the new value. The charge point responds to confirm whether the change was successful or if an error occurred. This helps manage charge point settings remotely.
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SetChangeConfigurationStatus | This function sets the status of the Change Configuration response based on the provided status value. | CHANGE_CONFIGURATION_STATUS_T status | void |
Example:
if((strcmp(key, "MeterValuesSampledData") == 0))
{
LogDebug("APP_LOG", " Reboot required to reflect change configuration..\n");
SetChangeConfigurationStatus(CHANGE_CONFIGURATION_REBOOT_REQUIRED);
}
else
{
SetChangeConfigurationStatus(CHANGE_CONFIGURATION_ACCEPTED);
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
ChangeConfigurationInit | This function initializes the Change Configuration response status to "Rejected" by default. | void | void |
Example:
void OCPPMessagesInit(void)
{
DataTransferInit();
ResetInit();
MeterValueStructInit();
SetLocalListVersionNumber(DEFAULT_SEND_LOCAL_LIST_VERSION);
SetChargePointConnectorId(CHARGEPOINT_DEFAULT_CONTROLLER);
SetChargePointError(NOERROR);
SetChargePointStatus(AVAILABLE);
SetAuthorizeStatus(AUTHORIZE_INVALID);
SetRemoteStartTransactionStatus(REMOTE_START_STOP_REJECTED);
SetOCPPWebsocketOnlineMode();
UnlockConnectorInit();
ReserveNowInit();
ChangeAvailabilityInit();
ClearCacheInit();
ChangeConfigurationInit();
CancelReservationInit();
GetAllIDsFromDB();
CheckAndStartClockAlignedMeterValueTimer();
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
GetChangeConfigurationParms | This function retrieves the key and value parameters from the received Change Configuration request. | char *key, char *value | void |
Example:
if((CHANGE_CONFIGURATION_STATUS_T)response == CHANGE_CONFIGURATION_ACCEPTED)
{
char key[CISTRING_50TYPE_LENGTH]; /* Key of the configuration changed. */
char value[CISTRING_500TYPE_LENGTH]; /* New value set of the configuration key. */
GetChangeConfigurationParms(key, value);
/* Below check just an example on how to handle reboot required w.r.t application requirement */
/* Below example explains whenever there is a change in MeterValuesSampledData configuration, then charepoint should
reboot to reflect the updated configuration */
if((strcmp(key, "MeterValuesSampledData") == 0))
{
LogDebug("APP_LOG", " Reboot required to reflect change configuration..\n");
SetChangeConfigurationStatus(CHANGE_CONFIGURATION_REBOOT_REQUIRED);
}
else
{
SetChangeConfigurationStatus(CHANGE_CONFIGURATION_ACCEPTED);
}
SendSetChargerConfigResponse();
}
|
Syntax |
Description |
Constants/Members |
|---|---|---|
CHANGE_CONFIGURATION_STATUS_T | This enum defines the possible statuses for a Change Configuration response. | CHANGE_CONFIGURATION_ACCEPTED CHANGE_CONFIGURATION_REJECTED CHANGE_CONFIGURATION_REBOOT_REQUIRED CHANGE_CONFIGURATION_NOT_SUPPORTED |
RX_CHANGECONFIGURATION_T | This structure contains the UUID, key and value for the Change Configuration request. | char uuid[]; char key[]; char value[]; |
char *ChangeConfigurationStatusType[] | Array to store the string representations of ChangeConfiguration statuses | Accepted Rejected RebootRequired NotSupported |
CHANGECONFIGURATION_RESPONSE_T | This structure contains the status of the Change Configuration response. | CHANGE_CONFIGURATION_STATUS_T status; |