3.27 Unlock Connector
The UnlockConnector message in OCPP 1.6J is sent by the central system to remotely unlock a specific connector, allowing the user to safely disconnect the charging cable. It specifies the connector ID of the connector to be unlocked. The charge point responds to confirm whether the unlock operation was successful. This feature is essential for user convenience and safety after a charging session.
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SetUnlockConnectorStatus | Sets the status for the UnlockConnector operation. | UNLOCK_CONNECTOR_STATUS_T status | void |
Example:
if(connectorDetails.connectorStatus == GOOD_CONNECTION)
{
char ChargePointStatus[CHARGE_POINT_STATUS_SIZE];
static char IdTag[CISTRING_20TYPE_LENGTH]={NULL_VALUE};
SetUnlockConnectorStatus(UNLOCK_CONNECTOR_UNLOCKED);
(void)SendUnlockConnectorResponse();
GetAuthorizeIdTag(IdTag);
GetChargePointStatus(ChargePointStatus);
LogDebug("APP_LOG", " charge point status:%s\n\r",ChargePointStatus);
if((strncmp(ChargePointStatus, "Charging", strlen(ChargePointStatus)) == 0) )
{
int transactionId;
LogDebug("APP_LOG", " UnlockConnector: Stop charging\n\r");
transactionId = GetStartTransactionResponseTransactionId();
UpdateAndSendStopTransaction(IdTag, OCPP_METER_READING, transactionId, UNLOCKCOMMAND, OCPP_KWH);
}
}
else
{
LogDebug("APP_LOG", " UnlockConnector: Bad connector connection\n\r");
SetUnlockConnectorStatus(UNLOCK_CONNECTOR_UNLOCKFAILED);
SendUnlockConnectorResponse();
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
UnlockConnectorInit | Initializes the UnlockConnector response parameters. | void | void |
Example:
void OCPPMessagesInit(void)
{
DataTransferInit();
ResetInit();
MeterValueStructInit();
SetLocalListVersionNumber(DEFAULT_SEND_LOCAL_LIST_VERSION);
SetChargePointConnectorId(CHARGEPOINT_DEFAULT_CONTROLLER);
SetChargePointError(NOERROR);
SetChargePointStatus(AVAILABLE);
SetAuthorizeStatus(AUTHORIZE_INVALID);
SetRemoteStartTransactionStatus(REMOTE_START_STOP_REJECTED);
SetOCPPWebsocketOnlineMode();
UnlockConnectorInit();
ReserveNowInit();
ChangeAvailabilityInit();
ClearCacheInit();
ChangeConfigurationInit();
CancelReservationInit();
GetAllIDsFromDB();
CheckAndStartClockAlignedMeterValueTimer();
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
GetUnlockConnectorParms | Retrieves the connector ID from the UnlockConnector request. | uint8_t *connectorId | void |
Example:
void UnlockConnector(uint16_t responsecode)
{
(void)responsecode;
uint8_t connectorId;
CONNECTOR_DETAILS connectorDetails;
GetUnlockConnectorParms(&connectorId);
LogDebug("APP_LOG", " UnlockConnector requested connectorId:%d\n\r",connectorId);
Syntax | Description | Constants/Members |
UNLOCKCONNECTOR_RESPONSE_T | Structure representing the response data for an UnlockConnector request | UNLOCK_CONNECTOR_STATUS_T status |
RX_UNLOCKCONNECTOR_T | Structure representing the request data for unlocking a connector | char uuid[]; uint8_t connectorId; |
UNLOCK_CONNECTOR_STATUS_T | Enumeration of possible statuses for the UnlockConnector operation | UNLOCK_CONNECTOR_UNLOCKED UNLOCK_CONNECTOR_UNLOCKFAILED UNLOCK_CONNECTOR_NOTSUPPORTED |