3.23 Reset
The Reset message in OCPP 1.6J is sent by the central system to restart or reset the charge point. It includes a reset type:
- Soft reset to reboot the charge point while keeping configurations.
- Hard reset to restore the charge point to factory settings.
The charge point responds to confirm whether the reset was successful or if there was an error. This helps resolve issues or apply new settings.
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SetResetStatus | Sets the status for the Reset request. | RESET_STATUS_T status | void |
Example:
case 'R': /*Rest*/
{
uint8_t resetState = 0;
LogDebug("APP_LOG", "Set Reset state: \n\t 0. Reset request accepted \n\t 1. Reset request rejected \n");
result = scanf("%hhd", (char*)&resetState);
if (result != 1)
{
LogDebug("APP_LOG", "Error reading ResetState\n");
}
if(resetState < 2U)
{
SetResetStatus(resetState);
(void)SendResetResponse();
}
}
break;
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
ResetInit | Initializes the Reset module. | void | void |
Example:
void OCPPMessagesInit(void)
{
DataTransferInit();
ResetInit();
MeterValueStructInit();
SetLocalListVersionNumber(DEFAULT_SEND_LOCAL_LIST_VERSION);
SetChargePointConnectorId(CHARGEPOINT_DEFAULT_CONTROLLER);
SetChargePointError(NOERROR);
SetChargePointStatus(AVAILABLE);
SetAuthorizeStatus(AUTHORIZE_INVALID);
SetRemoteStartTransactionStatus(REMOTE_START_STOP_REJECTED);
SetOCPPWebsocketOnlineMode();
UnlockConnectorInit();
ReserveNowInit();
ChangeAvailabilityInit();
ClearCacheInit();
ChangeConfigurationInit();
CancelReservationInit();
GetAllIDsFromDB();
CheckAndStartClockAlignedMeterValueTimer();
}
|
Syntax |
Description |
Constants/Members |
|---|---|---|
RESET_RESPONSE_T | Structure to hold the response of a Reset request | RESET_STATUS_T status |
RX_RESET_T | Structure to hold the details of a received Reset request | char uuid[]; RESET_TYPE_T typeENUM; |
RESET_TYPE_T | Enum representing the type of reset | RESET_HARD RESET_SOFT |
RESET_STATUS_T | Enum representing the status of a reset request | RESET_ACCEPTED RESET_REJECTED |