7.3.3.1 General
-Wl,optionPass
optionas an option to the linker. If theoptioncontains commas, it splits into multiple options at the commas. You can use this syntax to pass an argument to the option. For example, `-Wl,-Map,output.map' passes `-Map output.map' to the linker.-Wl, -nostartfilesDo not use the standard system startup files when linking. The standard system libraries are normally used unless
-nostdlibor-nodefaultlibsis used.-Wl,-nodefaultDo not use the standard system libraries when linking. Only the specified libraries will be passed to the linker. Options specifying linkage of the system libraries, such as
-static-libgccor -shared-libgcc, will be ignored. Usually, the standard start-up files are used, unless using-nostartfiles. The compiler may generate calls tomemcmp,memset,memcpy, andmemmove. These entries are usually resolved by entries in libc and should be supplied through some other mechanism when this option is specified.-Wl,-nostdlibDo not use the standard system start-up files or libraries when linking.
One of the standard libraries bypassed by
-nostdliband-nodefaultlibsislibgcc.a, a library of internal subroutines that GCC uses to overcome shortcomings of particular machines or special needs for some languages. In most cases, you need libgcc.a even when avoiding other standard libraries. In other words, when you specify -nostdlibor-nodefaultlibs, you should usually specify -lgcc as well to ensure that you have no unresolved references to internal GCC library subroutines.-Wl,-sRemove all symbol table- and relocation information from the executable.
-Wl,-staticOn systems that support dynamic linking, this prevents linking with the shared libraries. On other systems, this option has no effect.
-Wl,-MapGenerates Map file.