6.8 Kit Mode Setting
Some kits operate with different modes. Use this window to change the mode.

The table below lists some examples of the possible choices.
| Select mode | Persistent | Resulting mode |
|---|---|---|
| Mass Storage | Yes | Auto, enumerating as a Mass Storage Device kit |
| DGI | Auto, enumerating as a DGI kit | |
| Mass Storage | No | Mass Storage, enumerating once as a Mass Storage Device kit before returning to the previous mode |
| DGI | DGI, enumerating once as a DGI kit before return to the previous mode |
Note: When the persistent mode is used, the kit will reboot into Auto mode since the persistent choice changes the kit default.