10.5.4 Run Behavior
Underneath the argument boxes, you can modify the tool behavior.
Use output window - when checking this box, the tool will output processing information to the Microchip Studio output window. Otherwise, the output will be suppressed.
Close on exit - when checking this box, the tool window, if any, will be automatically closed after completing all operations.
Prompt for arguments - used for toolchain automation. The external tool will require user intervention to input additional processing parameters if the box is checked. Otherwise, the tool will be silent.
Treat output as Unicode - internationalization option. Some tools can output Unicode results for better interpretation. This option allows for correct output rendering if you are using such a tool.