12.4.1 How Do I Get My Tool to be Recognized by Microchip Studio?
This may happen automatically, but sometimes the Windows® driver does not recognize the tool correctly. To correct this, you have to check that the tool is listed under the Microchip node in the device manager in Windows. If your tool is not listed, try to find it under Unknown devices. If located there, try to reinstall the driver by double clicking the tool, clicking the Driver tab, and choosing Update Driver. Let Windows search for the driver. The driver may be reinstalled, and the tool displayed under Microchip. Now, the tool may be usable from Microchip Studio.