14.3.1 User Application Padding and Signature Alignment
When the Secure boot mode is enabled, padding is always inserted between the user application and its signature so the offset of this signature in internal Flash is always aligned to 128 bits. The padding is included in the computation of the user application signature.
In the sections that follow, the 128-bit aligned user signature refers to the user signature plus its padding.