1.3.2.4.8 I2C_BB_TransferSetup Function
C
bool I2C_BB_TransferSetup(I2CBB_TRANSFER_SETUP* setup, uint32_t tmrSrcClkFreq )Summary
Dynamic setup of I2C Bit Bang Library.
Description
This API is generally used when there are multiple clients on the same I2C bus having different I2C clock speed. In such a case, the I2C_BB_TransferSetup API must be called to set the appropriate I2C bus speed before starting the I2C transfer for the I2C slave.
Precondition
I2C_BB_Initialize must have been called for the associated I2C instance. The transfer status should not be busy.
Parameters
| Param | Description |
|---|---|
| setup | Pointer to the structure containing the transfer setup. |
| tmrSrcClkFreq | Timer Peripheral Clock Source Frequency. |
Returns
true - Transfer setup was updated Successfully.
false - Failure while updating transfer setup.
Example
I2C_TRANSFER_SETUP setup; setup.clkSpeed = 400000; // Make sure that the I2C is not busy before changing the I2C clock frequency if (I2C_BB_IsBusy() == false) { if (I2C_BB_TransferSetup( &setup, 0 ) == true) { // Transfer Setup updated successfully } }
Remarks
The timer period will be changed based on the new I2C clock speed, when an I2C request is submitted