1.3.2.4.3 I2C_BB_Write Function
C
bool I2C_BB_Write(uint16_t address, uint8_t *pdata, size_t length)Summary
Writes data to the slave.
Description
This function writes data to a slave on the bus. The function will attempt to write length number of bytes from pdata buffer to a slave whose address is specified by address. The I2C Master will generate a Start condition, write the data and then generate a Stop Condition. If the slave NAKs the request the transfer is terminated. The application can call the I2C_BB_ErrorGet() function to know that cause of the error.
The function is non-blocking. It initiates bus activity and returns immediately. The transfer is then completed in the timer peripheral interrupt. A transfer request cannot be placed when another transfer is in progress. Calling the write function when another function is already in progress will cause the function to return false.
The library will call the registered callback function when the transfer has terminated.
Precondition
I2C_BB_Initialize must have been called for the associated I2C instance.
Parameters
| Param | Description |
|---|---|
| address | 7-bit / 10-bit slave address. |
| pdata | pointer to source data buffer that contains the data to be written. |
| length | length of data buffer in number of bytes. Also the number of bytes to be written. |
Returns
true - The request was placed successfully and the bus activity was initiated.
false - The request fails,if there was already a transfer in progress when this function was called.
Example
uint8_t myData [NUM_BYTES]; void MyI2CCallback(uintptr_t context) { // This function will be called when the transfer completes. Note // that this function executes in the context of the I2C interrupt. } I2C_BB_Initialize(); I2C_BB_CallbackRegister(MyI2CCallback, NULL); if(I2C_BB_Write( SLAVE_ADDR, &myData[0], NUM_BYTES ) == false) { // error handling }
Remarks
None.