1.1.2.2 Using the Library

The I2C driver builds on top of the I2C Peripheral Library (PLIB) and provides write, read and write-read APIs in Blocking and Non-blocking mode for I2C host functionality.

  • Provides Write, Read and Write followed by Read APIs.

  • Supports multiple clients connected to the same I2C peripheral instance (Multi-client mode).

  • In Asynchronous (non-blocking) mode, application can either register a callback to get notified once the data transfer is complete or can poll the status of the data transfer using the status APIs.

  • In Asynchronous mode, application can queue more than one transmit/receive requests without waiting for the previous request to be completed. The number of transmit/receive requests that can be queued depends on the depth of the transfer queue configured using the MCC.

  • The Asynchronous mode is supported in both Bare-Metal and RTOS environment.

  • The Synchronous (blocking) mode of the driver is supported only in an RTOS environment.

  • The Synchronous mode of the driver does not support callback or queuing multiple requests. This is because the implementation is blocking in nature.

Example Application to Read and Write From I2C EEPROM in Asynchronous mode

#define APP_EEPROM_MEMORY_ADDR                  0x0000

/* Size of the string written to EEPROM must be less than or equal to the EEPROM page size */
#define APP_EEPROM_TEST_DATA                    "I2C EEPROM Demo"
#define APP_EEPROM_TEST_DATA_SIZE               (sizeof(APP_EEPROM_TEST_DATA)-1)
#define APP_EEPROM_RX_BUFFER_SIZE               APP_EEPROM_TEST_DATA_SIZE

#if APP_EEPROM_ADDR_LEN_BITS == 18 || APP_EEPROM_ADDR_LEN_BITS == 16
    /* For 18 bit address, A16 and A17 are part of the EEPROM slave address.
     * The A16 and A17 bits are set to 0 in this demonstration. */
    #define APP_EEPROM_NUM_ADDR_BYTES           2
#elif APP_EEPROM_ADDR_LEN_BITS == 8
    #define APP_EEPROM_NUM_ADDR_BYTES           1
#endif

#define APP_EEPROM_TX_BUFFER_SIZE        (APP_EEPROM_TEST_DATA_SIZE + APP_EEPROM_NUM_ADDR_BYTES)

APP_DATA appData;

static uint8_t testTxData[APP_EEPROM_TX_BUFFER_SIZE] = {0};
static uint8_t testRxData[APP_EEPROM_RX_BUFFER_SIZE] = {0};

void APP_I2CEventHandler (
    DRV_I2C_TRANSFER_EVENT event,
    DRV_I2C_TRANSFER_HANDLE transferHandle,
    uintptr_t context
)
{
    APP_TRANSFER_STATUS* transferStatus = (APP_TRANSFER_STATUS*)context;

    if (event == DRV_I2C_TRANSFER_EVENT_COMPLETE)
    {
        if (transferStatus)
        {
            *transferStatus = APP_TRANSFER_STATUS_SUCCESS;
        }
    }
    else
    {
        if (transferStatus)
        {
            *transferStatus = APP_TRANSFER_STATUS_ERROR;
        }
    }
}

void APP_Initialize ( void )
{
    /* Initialize the appData structure. */
    appData.state = APP_STATE_INIT;
    appData.drvI2CHandle   = DRV_HANDLE_INVALID;
    appData.transferHandle = DRV_I2C_TRANSFER_HANDLE_INVALID;
    appData.transferStatus = APP_TRANSFER_STATUS_ERROR;

#if APP_EEPROM_NUM_ADDR_BYTES == 2
    testTxData[0] = (APP_EEPROM_MEMORY_ADDR >> 8);
    testTxData[1] = APP_EEPROM_MEMORY_ADDR;
    memcpy(&testTxData[2], (const void*)APP_EEPROM_TEST_DATA, APP_EEPROM_TEST_DATA_SIZE);
#else
    testTxData[0] = APP_EEPROM_MEMORY_ADDR;
    memcpy(&testTxData[1], (const void*)APP_EEPROM_TEST_DATA, APP_EEPROM_TEST_DATA_SIZE);
#endif

}

void APP_Tasks ( void )
{
    /* Check the application's current state. */
    switch ( appData.state )
    {
        /* Application's initial state. */
        case APP_STATE_INIT:

            /* Open the I2C Driver */
            appData.drvI2CHandle = DRV_I2C_Open( DRV_I2C_INDEX_0, DRV_IO_INTENT_READWRITE );
            if(appData.drvI2CHandle == DRV_HANDLE_INVALID)
            {
                appData.state = APP_STATE_ERROR;
            }
            else
            {
                /* Register the I2C Driver event Handler */
                DRV_I2C_TransferEventHandlerSet(
                    appData.drvI2CHandle,
                    APP_I2CEventHandler,
                    (uintptr_t)&appData.transferStatus
                );
                appData.state  = APP_STATE_IS_EEPROM_READY;
            }
            break;

        case APP_STATE_IS_EEPROM_READY:

            appData.transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
            /* Add a dummy write transfer request to verify whether EEPROM is ready */
            DRV_I2C_WriteTransferAdd(
                appData.drvI2CHandle,
                APP_EEPROM_SLAVE_ADDR,
                (void *)&appData.dummyData,
                1,
                &appData.transferHandle
            );

            if( appData.transferHandle == DRV_I2C_TRANSFER_HANDLE_INVALID )
            {
                appData.state = APP_STATE_ERROR;
            }
            else
            {
                appData.state = APP_STATE_DATA_WRITE;
            }
            break;

        case APP_STATE_DATA_WRITE:
            if (appData.transferStatus == APP_TRANSFER_STATUS_SUCCESS)
            {
                appData.transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;

                /* Add a request to write the application data */
                DRV_I2C_WriteTransferAdd(
                    appData.drvI2CHandle,
                    APP_EEPROM_SLAVE_ADDR,
                    (void *)&testTxData[0],
                    APP_EEPROM_TX_BUFFER_SIZE,
                    &appData.transferHandle
                );

                if( appData.transferHandle == DRV_I2C_TRANSFER_HANDLE_INVALID )
                {
                    appData.state = APP_STATE_ERROR;
                }
                else
                {
                    appData.state = APP_STATE_WAIT_WRITE_COMPLETE;
                }
            }
            else if (appData.transferStatus == APP_TRANSFER_STATUS_ERROR)
            {
                //EEPROM is not ready. Keep checking until it is ready to receive commands.
                //Some EEPROMs need stabilization time before they can start responding to commands.
                appData.state = APP_STATE_IS_EEPROM_READY;
            }
            break;

        case APP_STATE_WAIT_WRITE_COMPLETE:
            if (appData.transferStatus == APP_TRANSFER_STATUS_SUCCESS)
            {
                appData.transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;

                /* Add a dummy write request to check if EEPROM's internal write cycle is complete */
                DRV_I2C_WriteTransferAdd(
                    appData.drvI2CHandle,
                    APP_EEPROM_SLAVE_ADDR,
                    (void *)&appData.dummyData,
                    1,
                    &appData.transferHandle
                );

                if( appData.transferHandle == DRV_I2C_TRANSFER_HANDLE_INVALID )
                {
                    appData.state = APP_STATE_ERROR;
                }
                else
                {
                    appData.state = APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS;
                }
            }
            else if (appData.transferStatus == APP_TRANSFER_STATUS_ERROR)
            {
                appData.state = APP_STATE_ERROR;
            }
            break;

        case APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS:
            if (appData.transferStatus == APP_TRANSFER_STATUS_SUCCESS)
            {
                appData.state = APP_STATE_DATA_READ;
            }
            else if (appData.transferStatus == APP_TRANSFER_STATUS_ERROR)
            {
                appData.transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;

                /* Keep checking if EEPROM's internal write cycle is complete */
                DRV_I2C_WriteTransferAdd(
                    appData.drvI2CHandle,
                    APP_EEPROM_SLAVE_ADDR,
                    (void *)&appData.dummyData,
                    1,
                    &appData.transferHandle
                );

                if( appData.transferHandle == DRV_I2C_TRANSFER_HANDLE_INVALID )
                {
                    appData.state = APP_STATE_ERROR;
                }
            }
            break;

        case APP_STATE_DATA_READ:

            appData.transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;

            /* Add a request to read data from EEPROM. */
            DRV_I2C_WriteReadTransferAdd(
                appData.drvI2CHandle,
                APP_EEPROM_SLAVE_ADDR,
                (void *)&testTxData[0],
                APP_EEPROM_NUM_ADDR_BYTES,
                (void *)&testRxData[0],
                APP_EEPROM_TEST_DATA_SIZE,
                &appData.transferHandle
            );

            if( appData.transferHandle == DRV_I2C_TRANSFER_HANDLE_INVALID )
            {
                appData.state = APP_STATE_ERROR;
            }
            else
            {
                appData.state = APP_STATE_WAIT_READ_COMPLETE;
            }
            break;

        case APP_STATE_WAIT_READ_COMPLETE:
            if (appData.transferStatus == APP_TRANSFER_STATUS_SUCCESS)
            {
                appData.state = APP_STATE_DATA_VERIFY;
            }
            else if (appData.transferStatus == APP_TRANSFER_STATUS_ERROR)
            {
                appData.state = APP_STATE_ERROR;
            }
            break;

        case APP_STATE_DATA_VERIFY:

            /* Compare data written and data read */
            if (memcmp(&testTxData[APP_EEPROM_NUM_ADDR_BYTES], &testRxData[0], APP_EEPROM_TEST_DATA_SIZE) == 0)
            {
                appData.state = APP_STATE_SUCCESS;
            }
            else
            {
                appData.state = APP_STATE_ERROR;
            }
            break;

        case APP_STATE_SUCCESS:

            appData.state = APP_STATE_IDLE;
            break;

        case APP_STATE_ERROR:

            appData.state = APP_STATE_IDLE;
            break;

        case APP_STATE_IDLE:
        default:
            break;
    }
}