1.6.3.2 DRV_G3ADP_MAC_Deinitialize Function
C
void DRV_G3ADP_MAC_Deinitialize(SYS_MODULE_OBJ object);
Summary
Deinitializes the G3 ADP Ethernet MAC.
Description
This function supports teardown of the G3 ADP MAC (opposite of set up). Used by tcpip_module_manager.
Precondition
DRV_G3ADP_MAC_Initialize() should have been called.
Parameters
| Param | Description |
|---|---|
| object | Driver object handle, returned from DRV_G3ADP_MAC_Initialize |
Returns
None.
Example
if(pNetIf->macObjHandle != 0)
{
DRV_G3ADP_MAC_Deinitialize(pNetIf->macObjHandle);
}
Remarks
It should be called to release any resources allocated by the initialization and disables callback functions with the G3 ADP layer.