1.6.3.4 DRV_G3ADP_MAC_Tasks Function

C

void DRV_G3ADP_MAC_Tasks( SYS_MODULE_OBJ object );

Summary

Maintains the G3 ADP MAC driver's state machine.

Description

This function is used to maintain the driver's internal state machine.

Precondition

The DRV_G3ADP_MAC_Initialize function must have been called before calling this function.

Returns

None.

Example

    if(pNetIf->macObjHandle != 0)
    {
        // process the underlying MAC module tasks
        DRV_G3ADP_MAC_Tasks(pNetIf->macObjHandle);
    }

Remarks

None.