1.6.3.10 DRV_G3ADP_MAC_PacketTx Function

C

TCPIP_MAC_RES DRV_G3ADP_MAC_PacketTx(DRV_HANDLE hMac, TCPIP_MAC_PACKET * ptrPacket);

Summary

G3 ADP MAC driver transmit function.

Description

This is the MAC transmit function. Using this function a packet is submitted to the G3 ADP stack for transmission.

Precondition

DRV_G3ADP_MAC_Initialize must have been called to set up the driver. DRV_G3ADP_MAC_Open() should have been called to obtain a valid handle.

Parameters

ParamDescription
hMacHandle identifying the MAC driver client
ptrPacketPointer to a TCPIP_MAC_PACKET that's completely formatted and ready to be transmitted over the network

Returns

  • TCPIP_MAC_RES_OK if success
  • A TCPIP_MAC_RES error value if failed

Example

    TCPIP_MAC_RES res;
    TCPIP_MAC_PACKET * ptrPacket;

    // The content of the packet must be built accordingly to TCPIP_MAC_PACKET
    if(pNetIf->hIfMac != 0)
    {
        res = DRV_G3ADP_MAC_PacketTx(pNetIf->hIfMac, ptrPacket);
    }

Remarks

  • The G3 ADP MAC driver supports internal queuing. A packet is rejected only if it is not properly formatted. Otherwise it will be scheduled for transmission and queued internally if needed.
  • Once the packet is scheduled for transmission the G3 ADP MAC driver will set the TCPIP_MAC_PKT_FLAG_QUEUED flag so that the stack is aware that this packet is under processing and cannot be modified
  • Once the packet is transmitted, the TCPIP_MAC_PKT_FLAG_QUEUED will be cleared, the proper packet acknowledgment result (ackRes) will be set and the packet acknowledgment function (ackFunc) will be called