1.6.3.18 DRV_G3ADP_MAC_EventAcknowledge Function
C
bool DRV_G3ADP_MAC_EventAcknowledge(DRV_HANDLE hMac, TCPIP_MAC_EVENT tcpAckEv);
Summary
Acknowledges and re-enables processed events.
Description
This function acknowledges and re-enables processed events. Multiple events can be ORed together as they are processed together. The events acknowledged by this function should be the events that have been retrieved from the stack by calling DRV_G3ADP_MAC_EventPendingGet() or have been passed to the stack by the driver using the registered notification handler and have been processed and have to be re-enabled.
Precondition
DRV_G3ADP_MAC_Initialize must have been called to set up the driver. DRV_G3ADP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Param | Description |
|---|---|
| hMac | Handle identifying the MAC driver client |
| tcpAckEv | The events that the user processed and need to be re-enabled |
Returns
- true if events acknowledged
- false if no events to be acknowledged
Example
TCPIP_MAC_EVENT activeEvents;
// Get Pending events
activeEvents = DRV_G3ADP_MAC_EventPendingGet(pNetIf->hIfMac);
// Process events
(...)
// Acknowledge events
DRV_G3ADP_MAC_EventAcknowledge( hMac, activeEvents );
Remarks
- All events should be acknowledged, in order to be re-enabled
- Some events are fatal errors and should not be acknowledged (TCPIP_MAC_EV_RX_BUSERR, TCPIP_MAC_EV_TX_BUSERR). Driver/stack re-initialization is needed under such circumstances.
- Some events are just system/application behavior and they are intended only as simple info (TCPIP_MAC_EV_RX_OVFLOW, TCPIP_MAC_EV_RX_BUFNA, TCPIP_MAC_EV_TX_ABORT, TCPIP_MAC_EV_RX_ACT)
- The events are persistent. They should not be re-enabled unless they have been processed and the condition that generated them was removed. Re-enabling them immediately without proper processing will have dramatic effects on system performance.