7.4.2 Instructions in Program Memory
The program memory is addressed in bytes. Instructions are stored as
         either two bytes, four bytes, or six bytes in program memory. The Least Significant Byte of
         an instruction word is always stored in a program memory location with an even address (LSb
         = 0). To maintain alignment with instruction boundaries, the PC increments
         in steps of two and the LSb will always read ‘0’. See the “Program
            Counter” section in the “Memory Organization” chapter for more details. The
         instructions in the Program Memory figure below shows how instruction words are stored in
         the program memory.
The CALL and GOTO instructions have the absolute program memory
         address embedded into the instruction. Since instructions are always stored on word
         boundaries, the data contained in the instruction is a word address. The word address is
         written to the corresponding bits of the Program Counter register, which accesses the
         desired byte address in program memory. Instruction #2 in the example shows how the
         instruction GOTO 0006h is encoded in the program
         memory. Program branch instructions, which encode a relative address offset, operate in the
         same manner. The offset value stored in a branch instruction represents the number of
         single-word instructions by which the PC will be offset.