43.3.6.9 Randomize a Coordinate
Purpose
This service is used to convert the projective representation of a point to another projective representation.
How to Use the Service
Description
The operation performed is:
Projective(X1, Y1, Z1) → Projective(X2, Y2, Z2)
In this computation, the following parameters need to be provided:
- The input point is filled in projective coordinates (X,Y,Z) (pointed by {nu1PointBase,3*u2ModLength + 12}). This Point must not be the point at infinity.
- Cns the Fast Modular Constant filled (pointed by {nu1CnsBase,u2ModLength +8})
- P the modulus filled (pointed by {nu1ModBase,u2ModLength +4})
- The workspace not initialized (pointed by {nu1WorkSpace, 3*u2ModLength +28}
- The random number (pointed by {nu1RandomBase, u2ModLength +4}).
The result is the point nu1PointBase with its (X,Y,Z) coordinates randomized.
The service for this operation is ZpEcRandomiseCoordinate.
- Ensure that the constant Cns has been calculated with the setup of the Modular Reduction service.
- Be sure to follow the directives given for the RNG on the chip you use (particularly initialization, seeding) and compulsorily start the RNG
Parameters Definition
| Parameter | Type | Direction | Location | Data Length | Before Executing the Service | After Executing the Service |
|---|---|---|---|---|---|---|
| nu1ModBase | nu1 | I | Crypto RAM | u2ModLength + 4 | Base of modulus P | Base of modulus P |
| nu1CnsBase | nu1 | I | Crypto RAM | u2ModLength + 8 | Base of Cns | Base of Cns |
| u2ModLength | u2 | I | – | – | Length of modulus P | Length of modulus P |
| nu1PointBase | nu1 | I | Crypto RAM | 3*u2ModLength + 12 | Input point | Resulting point |
| nu1RandomBase | nu1 | I | Crypto RAM | u2ModLength + 4 | Random | Corrupted |
| nu1Workspace | nu1 | I | Crypto RAM | 3*u2ModLength + 28 | – | Workspace |
Code Example
PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;
// ! The Random Number Generator must be initialized and started
// ! following the directives given for the RNG on the chip
PUKCL (u2Option) = 0;
// Depending on the option specified, not all fields should be filled
PUKCL _ZpEccRandomiseCoordinate(nu1ModBase) = <Base of the ram location of P>;
PUKCL _ZpEccRandomiseCoordinate(u2ModLength) = <Byte length of P>;
PUKCL _ZpEccRandomiseCoordinate(nu1CnsBase) = <Base of the ram location of Cns>;
PUKCL_ZpEccRandomiseCoordinate(nu1RandomBase) = <Base of the ram location where the the RNG is stored>;
PUKCL _ZpEccRandomiseCoordinate(nu1PointBase) = <Base of the ram location of the point>;
PUKCL _ZpEccRandomiseCoordinate(nu1Workspace) = <Base of the ram location of the workspace>;
...
// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library...
vPUKCL_Process(ZpEccRandomiseCoordinate,&PUKCLParam);
if (PUKCL (u2Status) == PUKCL_OK)
{
...
}
else // Manage the error
Constraints
No overlapping between either input and output are allowed. The following conditions must be avoided to ensure that the service works correctly:
- nu1ModBase, nu1CnsBase, nu1PointABase, nu1RandomBase, nu1Workspace are not aligned on 32-bit boundaries
- {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1RandomBase, u2ModLength + 4}, {nu1Workspace, <WorkspaceLength>} are not in Crypto RAM
- u2ModLength is either: < 12, > 0xffc or not a 32-bit length
- All overlapping between {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength +8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1RandomBase, u2ModLength + 4} and {nu1Workspace, 3*u2ModLength + 28}
Status Returned Values
| Returned Status | Importance | Meaning |
|---|---|---|
| PUKCL_OK | – | The computation passed without problem. |