43.3.3.6 Return Codes
Each call to one of the PUKCL services returns a status code indicating whether or not the execution is correct, which can be decoded, as shown in the following figure.

The following table shows how the severity indicators should be decoded.
| Value for Bits 14–15 | Severity | Comment |
|---|---|---|
| 0xC000 | Severe | Indicates a blocking error condition |
| 0x8000 | Warning | Indicates a cautionary use of the return values |
| 0x4000 | Information | Indicates the result is correct and gives information |
| 0x0000 | – | No error or no severity given |
The following table contains the exhaustive list of all reason codes.
| Value for Bits 00–13 | Severity Code | Reason Code |
|---|---|---|
| 0x0000 | – | PUKCL_OK |
| 0x4001 | Informative | PUKCL_NUMBER_IS_NOT_PRIME |
| 0x4002 | Informative | PUKCL_NUMBER_IS_PRIME |
| 0xC001 | Severe | PUKCL_COMPUTATION_NOT_STARTED |
| 0xC002 | Severe | PUKCL_UNKNOWN_SERVICE |
| 0xC003 | Severe | PUKCL_UNEXPLOITABLE_OPTIONS |
| 0xC004 | Severe | PUKCL_HARDWARE_ISSUE |
| 0xC005 | Severe | PUKCL_WRONG_HARDWARE |
| 0xC006 | Severe | PUKCL_LIBRARY_MALFORMED |
| 0xC007 | Severe | PUKCL_ERROR |
| 0xC008 | Severe | PUKCL_UNKNOWN_SUBSERVICE |
| 0xC101 | Severe | PUKCL_DIVISION_BY_ZERO |
| 0xC102 | Severe | PUKCL_MALFORMED_MODULUS |
| 0xC103 | Severe | PUKCL_FAULT_DETECTED |
| 0xC104 | Severe | PUKCL_MALFORMED_KEY |
Please note the following rules about return codes:
- A status value indicating a severe error, means that an expected operation has not been executed or has been corrupted. Therefore, the result of such an operation should never be used.
- A status value indicating a warning should be looked at precisely, as the expected correctness of the result cannot be guaranteed.
- A status value indicating an information always means that the result is correct with no possible misinterpretation of the values.
- A status value zero indicates that there is no error or no severity.
In the following sections, for each service, the constraints on the parameters placement are detailed. For reduced code size and higher execution speed, tests are processed on these constraints. It is important that PUKCL users take these placement constraints into consideration at the development and test stages to ensure the correct functioning of the library.