43.3.7.10 Verifying an ECDSA Signature (Compliant with FIPS 186-2)
Purpose
This service is used to verify an ECDSA signature following the FIPS 186-2. It performs the second step of the Signature Verification.
A hash value (HashVal) must be provided as input, it has to be previously computed from the message to be signed using a secure hash algorithm.
As second significant input, the Signature is provided to be checked. This service checks the signature and fills the status accordingly.
How to Use the Service
Description
The operation performed is:
Verify = EcDsaVerifySignature(PtA, HashVal, Signature, CurveParameters, PublicKey)
The points used for this operation are represented in different coordinate systems. In this computation, the following parameters need to be provided:
- A the input point is filled with the affine values (X,Y) and Z = 1 (pointed by{nu1PointABase,3*u2ModLength + 12})
- Cns the working space for the Fast Modular Constant not initialized (pointed by {nu1CnsBase,u2ScalarLength + 8})
- P the modulus filled (pointed by {nu1ModBase,u2ModLength +4})
- The workspace not initialized (pointed by {nu1WorkSpace, 8*u2ModLength +44} The a and b parameters relative to the elliptic curve (pointed by {nu1ABase,2*u2ModLength + 8})
- The order of the Point A on the elliptic curve (pointed by {nu1OrderPointBase,u2ScalarLength +4})
- HashVal the hash value beforehand generated and filled (pointed by {nu1HashBase,u2ScalarLength +4})
- The Public Key point is filled in “mixed” coordinates (X,Y) with the affine values and Z = 1 (pointed by {nu1PointPublicKeyGen, 3*u2ModLength + 12})
- The input
signature (R,S), even if it is not a Point, is represented
in memory like a point in affine coordinates (X,Y) (pointed
by {nu1PointSignature, 2*u2ScalarLength + 8})Important: For the ECDSA signature verification be sure to follow the directives given for the RNG on the chip you use (particularly initialization, seeding) and compulsorily start the RNG.
- The operation consists in obtaining a V value with all these input parameter and check that V equals the provided R. If all is correct and the signature is the good one, the status is set to PUKCL_OK. If all is correct and the signature is wrong, the status is set to PUKCL_WRONG_SIGNATURE. If an error occurs, the status is set to the corresponding error value (see Status Returned Values below).
The service name for this operation is
GF2NEcDsaVerifyFast. This service uses Fast
mode and Fast Modular Reduction for computation.
Parameters Definition
| Parameter | Type | Direction | Location | Data Length | Before Executing the Service | After Executing the Service |
|---|---|---|---|---|---|---|
| nu1ModBase | nu1 | I | Crypto RAM | u2ModLength + 4 | Base of modulus P | Base of modulus P |
| nu1CnsBase | nu1 | I | Crypto RAM | u2ScalarLength + 8 | Base of Cns | Base of Cns |
| u2ModLength | u2 | I | – | – | Length of modulus P | Length of modulus P |
| nu1OrderPointBase | nu1 | I | Crypto RAM | u2ScalarLength + 4 | Order of the Point A in the elliptic curve | Unchanged |
| nu1PointSignature | nu1 | I | Crypto RAM | 2*u2ScalarLength + 8 | Signature(r, s) | Corrupted |
| nu1HashBase (see Note 1) | nu1 | I | Crypto RAM | u2ScalarLength + 4 | Base of the hash value resulting from the previous SHA | Corrupted |
| u2ScalarLength | u2 | I | – | – | Length of scalar | Length of scalar |
| nu1PointABase | nu1 | I/O | Crypto RAM | 3*u2ModLength + 12 | Generator point | Corrupted |
| nu1PointPublicKeyGen | nu1 | I/O | Crypto RAM | 3*u2ModLength + 12 | Public point | Corrupted |
| nu1ABase | nu1 | I | Crypto RAM |
2*u2ModLength + 8 | Parameter a and b of the elliptic curve | Unchanged |
| nu1Workspace | nu1 | I | Crypto RAM | 8*u2ModLength + 44 | – | Corrupted workspace |
- Whatever the chosen SHA, the resulting hash value may have a length inferior or equal to the modulo length and be padded with zeros until its total length is u2ModLength + 4.
Code Example
PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;
// ! The Random Number Generator must be initialized and started
// ! following the directives given for the RNG on the chip
PUKCL (u2Option) = 0;
// Depending on the option specified, not all fields should be filled PUKCL _GF2NEcDsaVerify(nu1ModBase) = <Base of the ram location of P>;
PUKCL _GF2NEcDsaVerify(u2ModLength) = <Byte length of P>;
PUKCL _GF2NEcDsaVerify(nu1CnsBase) = <Base of the ram location of Cns>;
PUKCL _GF2NEcDsaVerify(nu1PointABase) = <Base of the A point>;
PUKCL _GF2NEcDsaVerify(nu1PrivateKey) = <Base of the Private Key>;
PUKCL _GF2NEcDsaVerify(nu1ScalarNumber) = <Base of the ScalarNumber>;
PUKCL _GF2NEcDsaVerify(nu1OrderPointBase) = <Base of the order of A point>;
PUKCL _GF2NEcDsaVerify(nu1ABase) = <Base of the a parameter of the curve>; PUKCL _GF2NEcDsaVerify(nu1Workspace) = <Base of the workspace>;
PUKCL _GF2NEcDsaVerify(nu1HashBase) = <Base of the SHA resulting hash>;
...
// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library...
vPUKCL_Process(GF2NEcDsaVerifyFast, &PUKCLParam);
if (PUKCL (u2Status) == PUKCL_OK)
{
...
}
else
if(PUKCL(u2Status) == PUKCL_WRONG_SIGNATURE)
{
...
}
else // Manage the error
Constraints
No overlapping between either input and output are allowed. The following conditions must be avoided to ensure the service works correctly:
- nu1ModBase, nu1CnsBase, nu1PointABase, nu1PointPublicKeyGen, nu1PointSignature, nu1OrderPointBase,nu1ABBase, nu1Workspace or nu1HashBase are not aligned on 32-bit boundaries
- {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1PointPublicKeyGen, 3*u2ModLength + 12}, {nu1PointSignature,2*u2ScalarLength + 8}, {nu1OrderPointBase, u2ScalarLength + 4}, {nu1ABBase, 2*u2ModLength + 8}, {nu1Workspace, <WorkspaceLength>} or {nu1HashBase, u2ScalarLength + 4} are not in Crypto RAM
- u2ModLength is either: < 12, > 0xffc or not a 32-bit length
- All overlapping between {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength +8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1PointPublicKeyGen, 3*u2ModLength + 12}, {nu1PointSignature, 2*u2ScalarLength + 8}, {nu1OrderPointBase, u2ScalarLength + 4}, {nu1ABBase, 2*u2ModLength + 8}, {nu1Workspace, <WorkspaceLength>} and {nu1HashBase, u2ScalarLength + 4}
Status Returned Values
| Returned Status | Importance | Meaning |
|---|---|---|
| PUKCL_OK | – | The computation passed without errors. The signature is correct. |
| PUKCL_WRONG_SIGNATURE | Warning | The signature is incorrect. |