49.6.2.1 Initialization
The following registers are
enable-protected, meaning that they can only be written when the TCC is disabled
(CTRLA.ENABLE = 0):
- The Control A (CTRLA) register, except Run Standby (RUNSTDBY), Enable (ENABLE) and Software Reset (SWRST) bits
- The Recoverable Fault n Control registers (FCTRLA and FCTRLB)
- The Waveform Extension Control register (WEXCTRL)
- The Drive Control register (DRVCTRL)
- The Event Control register (EVCTRL)
Enable-protected bits in the CTRLA register can be written simultaneously as CTRLA.ENABLE is written to '1', but not at the same time as CTRLA.ENABLE is written to '0'. Enable-protection is denoted by the ‘Enable-Protected’ property in the register description.
Before enabling the TCC, follow these steps
to configure it:
- Enable the TCC bus clock (CLK_TCCx_APB).
- If Capture mode is required, enable the channel in Capture mode by writing a '1' to the Capture Enable bit in the Control A register (CTRLA.CPTEN).
Optionally, the following configurations
can be set before enabling TCC:
- Select PRESCALER setting in the Control A register (CTRLA.PRESCALER).
- Select Prescaler Synchronization setting in the Control A register (CTRLA.PRESCSYNC).
- If down-counting operation is desired, write the Counter Direction bit in the Control B Set register (CTRLBSET.DIR) to '1'.
- Select the Waveform Generation operation in the WAVE register (WAVE.WAVEGEN).
- Select the Waveform Output Polarity in the WAVE register (WAVE.POL).
- The waveform output can be inverted for the individual channels using the Waveform Output Invert Enable bit group in the Driver register (DRVCTRL.INVEN).