2.14.2 Wi-Fi®

Potential issue whereby the DMA interface module can latch the sub-MSDU length for an A-MSDU from the header as a frame is received but before the FCS is validated. Because of this, an incorrect length could be latched for a corrupted received frame (A-MSDU or not). When latched, this length is updated only on the reception of a valid A-MSDU.

This can cause the receiver to lock up. This issue is fixed in the B0 silicon revision by adding logic to clear the latched sub-MSDU length field.

Work Around

None.

Affected Silicon Revisions

A0A1B0C0
X