1.4 CAN FD Blocking
This example application shows how to use the CAN module to transmit and receive CAN FD messages in polling mode.
Description
This application transmits CAN FD message to CAN Bus and receives CAN FD message from CAN Bus. To run this application, two evaluation boards of same type are required. These boards acts as different nodes on the CAN bus. Same application is programmed onto both the boards. Boards are connected to PC via UART. While running the application, user can send and receive CAN FD messages between the boards using UART console applications running on the PC.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/can/can_fd_operation_blocking/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mz_w1_curiosity.X | MPLABX project for PIC32MZ W1 Curiosity Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mz_w1_curiosity.X | PIC32MZ W1 Curiosity Board |
Setting Up PIC32MZ W1 Curiosity Board
- Connect ATA6563 click board to the PIC32MZ W1 Curiosity
Board for each board as per the Pin connections shown below
PIC32MZ W1 Curiosity Board ATA6563 click board PIN14 (RPB9), mikroBUS Connector RX (PIN 14) PIN13 (RPB7), mikroBUS Connector TX (PIN 13) +3.3V, mikroBUS Connector 3V3 (PIN 7) +5V, mikroBUS Connector 5V (PIN 10) GND, mikroBUS Connector GND (PIN 9) - Connect ATA6563 click board-1 to ATA6563 click board-2 using female to female DB9 serial cable
- Connect the USB to TTL serial (USB UART click board) to U1TX pin (pin 23) and U1RX pin (pin 13) of J207 header for each board
- Connect the Debug USB port on the board to the computer using a mini USB cable for each board
- Connect mini USB cable to USB UART click board to the computer for each board (This will enumerate the USB to UART port)
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the DEBUG UART Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application using its IDE
- In the console associated with board 2, press “3” to receive a CAN FD message
- In the console associated with board 1, press “2” to transmit a CAN FD message
- Transmitted message description and status will be displayed in the console window of board 1
- Received message will be displayed in the console window of board 2
- Follow the sequence below to send and receive different messages:
- Press ‘3’ on board 2 and Press ‘2’ on board 1
- Press ‘3’ on board 2 and Press ‘1’ on board 1
- Press ‘3’ on board 2 and Press ‘2’ on board 1
- If the steps are executed in this sequence, the final output in the consoles
will be as below (console on the left is the transmitter (board 1) and the one
on the right is receiver (board 2)):