2.7 Generic USB Device Library

Topics

Name Description
IntroductionIntroduces the MPLAB Harmony Generic USB Device Library.
Using the Library This topic describes the basic architecture of the Generic USB Device Library and provides information and examples on its use.
Configuring the LibraryDescribes how to configure the Generic USB Device Library.
Library InterfaceThe API for implementing the Generic USB Device is contained the USB Device Library. Please refer to the Library Interface section in the USB Device Layer Library for more details.