2.4 USB Audio 2.0 Device Library

Topics

Name Description
IntroductionThis section provides information on library design, configuration, usage and the library interface for the USB Audio 2.0 Device Library.
Using the LibraryThis topic describes the basic architecture of the Audio 2.0 Function Driver and provides information and examples on its use.
How the Library Works This section explains the working of the Audio 2.0 Function Driver Library.
Configuring the LibraryThe application designer must specify the following configuration parameters while using the USB Audio 2.0 Device Driver. The configuration macros that implement these parameters must be located in the system_config.h file in the application project and a compiler include path (to point to the folder that contains this file) should be specified.
Library InterfaceThis section describes the Application Programming Interface (API) functions of the USB Device Audio LibraryRefer to each section for a detailed description.
FilesThis section lists the source and header files used by the library.